Absolute Maximum Ratings for XTALI pin of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Absolute Maximum Ratings for XTALI pin of i.MX6

Jump to solution
689 Views
yuuki
Senior Contributor II

Dear all,

We want to connect 24MHz oscillator to a XTALI pin.

We found DC Parameter for the  XTALI pin.
However we couldn't find absolute maximum rating of this pin.

Could you teach the absolute maximum rating for XTALI pin?

Best Regards,
Yuuki Murasato

Labels (1)
0 Kudos
1 Solution
526 Views
art
NXP Employee
NXP Employee

The minimum allowed voltage on the XTALI pin is -0.2V, the maximum voltage must not exceed NVCC_PLL_OUT.


Have a great day,
Artur
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
527 Views
art
NXP Employee
NXP Employee

The minimum allowed voltage on the XTALI pin is -0.2V, the maximum voltage must not exceed NVCC_PLL_OUT.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos