Whitch mean description of clock frequency.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Whitch mean description of clock frequency.

Jump to solution
627 Views
takashitakahash
Contributor III

Description of IMX6SDL RM of  61.8.4.2 DIV2, PSR and PM Bit Description.

Description of [ NOTE

You must ensure that the bit-clock frequency must be never

greater than 1/5 of the peripheral clock frequency. The

oversampling clock frequency can go up to peripheral clock

frequency.]

This description of "Peripheral clock"are the ssi_clk_root or ipg_clk_root ?

Labels (1)
0 Kudos
1 Solution
492 Views
Yuri
NXP Employee
NXP Employee

  According to Table 61-3 (SSI Clocks) of the RM, ipg_clk_root is peripheral clock

SSI_clcoks.jpg


Have a great day,
Yuri
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
493 Views
Yuri
NXP Employee
NXP Employee

  According to Table 61-3 (SSI Clocks) of the RM, ipg_clk_root is peripheral clock

SSI_clcoks.jpg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos