AnsweredAssumed Answered

i.MX28 Video playback issue

Question asked by ryan lee on Nov 28, 2014

I am a video playback test using i.mx28 ref B/D and IMX28 L2.6.35_1.1.0_130130_source code.
But I can't see video screen only hear MP3 audio.

 

<Installation Procedure>
1. ltib is installed Gnome packages using IMX28 L2.6.35_1.1.0_130130_source.
2. Installed  L2.6.35_1.1.0_130130_MM_CODECS_BUNDLE.
gst-fsl-plugins-3.0.6.tar.gz
libfslcodec-3.0.6.tar.gz
libfslparser-3.0.6.tar.gz
3. ltib -C
Package list -> Freescale Multimedia Plugins/Codecs  ---> [*] gst-fsl-plugins
4. Video playback test after scouce code complie but can't see video.

But If when I use another demo image file, Video playback is OK.

 

Pls refer to attached file of video playback test log message and mov1.avi video test file.

One is video playback OK.
Another log file is video playback NG.
You can see the different library versions.

 

Pls comment helpful for resolve this problem.

Original Attachment has been moved to: Video_NG_Image_log.txt.zip

Original Attachment has been moved to: Video_OK_Image_log.txt.zip

Outcomes