AnsweredAssumed Answered

How to flash the freescale Linux image to the SD card? (i.MX28 EVK)

Question asked by Christoph Kobe on Nov 28, 2014
Latest reply on Nov 28, 2014 by Pt A R

Hi,

 

we own a i.MX28 EVK and I switched of the Board while Linux was running - now the ext2 filesystem is broken and the gui doesn't come up.

 

I would like to bring the SD card to the "factory default", as it was delivered with the evaluation kit. I already downloaded

  1. CFImager.v1.7.3.001_bin+src
  2. L2.6.35_1.1.0_130130_images_MX28

but now I'm stuck and don't know how to use the tool and the files. I tried

 

CFImager.exe -d f -f rootfs.ext2

and

CFImager.exe -d f -f imx28_uboot.sb

 

but in both cases when I insert the card into the i.MX28 EVK the serial console just outputs a hexadecimal number instead of booting, e.g.

0x80502008

 

How can I write the Linux Image that was shipped with the board to a SD card?

 

Thanks

Christoph

Outcomes