trouble on MM9Z1_638D1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

trouble on MM9Z1_638D1

624 Views
dwei
Contributor I

Hello.all

I am working with MM9Z1_638D1 .freshman. So far I was even unable to download the procedure.When i  downloaded the procedure with  CW10.6,meeted

17061_17061.png捕获.PNG.png

Then i click “yes”,and meet

17060_17060.pngQQ截图20141128103821.png

and then i follow the prompts,

but meet that"device is secure,erase to unsecure"again,i click yes again and meet

17062_17062.pngQQ截图20141128104647.png

and i click retry ,but it dosent work

Labels (1)
0 Kudos
2 Replies

423 Views
GordonD
Contributor IV

If you are using the KIT9Z1J636EVM and the OSBDM that is on the EVM, switch S1 must be set as follows:

OSBDM S1.png

If an External BDM tool is being used (i.e. USB Multilink), S1 must be configured as follows:

External BDM.png

Hope this helps.

0 Kudos

423 Views
ahmedfawad
Contributor I

which board u r using ?

0 Kudos