Has anybody tried multiple bluetooth connections on Nitrogen6x in Android 4.3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has anybody tried multiple bluetooth connections on Nitrogen6x in Android 4.3?

521 Views
tyrelbenson
Contributor I

I'm trying to get multiple serial bluetooth connections working on Android 4.3 on a Nitrogen6x.  I have a working Android app but I seem to be capped at 5 connections.  Is this a limitation of Android or am I missing something?

Labels (1)
Tags (1)
0 Kudos
1 Reply

418 Views
SergioSolis
NXP Employee
NXP Employee

I'm not that familiar with the nitrogen6x, but I saw that it uses the TiWi-BLE chip. Bluetooth connection limits is dependant on hardware rather than software. According to the TiWi-BLE engineer, it supports up to 7 connections (someone said 6).

I would recommend that you check the bluetooth driver, it may need an upgrade to the latest driver.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos