Dear,
After reading below discussion in Freescale community, Freescale people mentioned someone enabled SDIO 3.0 and we can contact local team for the issue. Could you help to share with us in the information about enabling SDIO 3.0 (customer/third party etc.)? Appreciated your help.
BR
Keith
Hi Keith
you can check attached files and link below
linux-2.6-imx.git - Freescale i.MX Linux Tree
Customer info is private and can not be shared, sorry.
Best regards
igor
Dear Igor,
Appreciated your help and information. Could you help to provide the information of following questions in advance? Thanks.
1) Did the test use real AP to get the throughput? If yes, could you provide the type/name of the real AP? We will reproduce the environment in our side.
2) Did the test use 2x2 MIMO in this throughput test?
3) Since BCM43241 supports 802.11 a/b/g/n, HS mode should be enough for support 802.11n, is it?
4) Do the patches of 'sabre ai sdio 3.0_patches.zip' be used to verify 802.11ac before?
Best regards
Keith