AnsweredAssumed Answered

P2020 support 36BIT, board.cfg options setting

Question asked by Kuowei Hsu on Nov 25, 2014
Latest reply on Nov 27, 2014 by Kuowei Hsu

Hi,

 

Our development board using p2020 needs to support 4G SDRAM. So we need CONFIG_36BIT enable.

In board.cfg, we add our config like

 

Status, Arch,     CPU:SPLCPU,    SoC,        Vendor,         Board name,         Target,                         Options,

Active  powerpc     mpc85xx          -             freescale        develop-1              DEVELOP-1                   -  

Active  powerpc     mpc85xx          -             freescale        develop-1              DEVELOP-1_36BIT      develop-1:36BIT

 

Q1: we have a develop-1.h under include/configs/ and folder develop-1 under board/freescale/. As I know the options format <board>:[other options], so I setting develop-1:36BIT. Is it correct??

 

Q2: we add DEVELOP-1 first and then DEVELOP-1_36BIT. If we want to build DEVELOP-1_36BIT, should we need to type from "bitbake -c cleansstate u-boot" or what command can we use to save our time build new configuration?? For example, bitbake -c clean <target>, bitbake -c cleansstate <target>, bitbake -c cleanall <target>.

 

At last, we using boot code not support 36BIT in our board which have a 4G SDRAM, then we see.

 

Not enough bank(chip-select) for CS0+CS1 on controller 0, interleaving disabled!

Detected 4 GiB of memory

       This U-Boot only supports < 4G of DDR

       You could rebuild it with CONFIG_PHYS_64BIT

       2 GiB (DDR3, 64-bit, CL=6, ECC off)

 

 

Thanks for any response.

 

Best Regard,

Kuowei Hsu

Outcomes