AnsweredAssumed Answered

Using Dual-LVDS I/F and RGB I/F by 2Display system

Question asked by Takashi Takahashi on Nov 20, 2014
Latest reply on Nov 27, 2014 by Joan Xie

Use the iMX6 Dual, we would like to drive the TFT resolution of 1920x720 and 800x480 resolution TFT resolution at the same time and same contents.

 

There are TFT interface, the 1920 x 720 are  Dual-LVDS and 800 x 480 are RGB24bit .

connection with iMX6 is connected to Dual-LVDS are LVDS0, 1 and RGB24bit are connected to the IPU1_DISP0.

At this time, 2 CH of the IPU Display I/f (DI) is assigned Dual-LVDS and RGB24bit each ?

 

In other words, Dual-LVDS data (DI), after entered into LVDS Display Bridge (LDB), divided by  even pixels and odd pixels after output from LVDS0 and LVDS1.

 

In my understand is correct ?

 

Outcomes