AnsweredAssumed Answered

The condition to occur MMPF0100 ER19.

Question asked by Satoshi Shimoda on Nov 20, 2014
Latest reply on Nov 20, 2014 by igorpadykov

Hi community,

 

I have a question about MMPF0100 ER19.

Please see ER19 in MMPF0100 errata sheet (Rev.4.0).

It says about the condition to occur this erratum as following.

=====

In applications without a valid voltage on the LICELL pin,

when VIN starts its ramp from between 100mV and 400mV,

there can be two failure symptoms:

=====

 

So I guess this erratum is not occurred if there is a valid voltage on LICELL pin when VIN starts its ramp from between 100mV and 400mV.

Is this correct?

Or there is a possibility to occur this erratum if VIN starts ramp from between 100mV and 400mV even though there is a valid voltage on LICELL pin?

 

Best Regards,

Satoshi Shimoda

Outcomes