Steve Baker

We bought the Graphic LCD Library driver package for the...

Discussion created by Steve Baker on Sep 24, 2007
Latest reply on Sep 25, 2007 by CrasyCat
We bought the Graphic LCD Library driver package for the KSO7xx family for use with CodeWarrior on 8 bit processors.  The package requires that we define a preprocessor compiler switch, GHW_SINGLE_CHIP (as in #define GHW_SINGLE_CHIP).  I've looked the documentation but have not found where to add this preprocessor compiler switch.  The company supplying the software said the following: "Compiler switches are usually defined on the command line, or if an Integrated Development Environment is used, in some parameter setup window for the compilation project.  Usually definition of compiler switches are located in the IDE near the place where you also can define additional include file paths for use during compilation."
 
We're "stuck in the mud" and can use some help.
 
Steve Baker

Outcomes