Hi. I have a question regarding the FXOS8700CQ 3-axis magentometer and accelerometer. I am considering using this sensor to detect the Earth's magnetic field in a device that can rotate as fast as 7200 degrees/s. Can the magnetometers respond fast enough to provide an accurate measurement when the magnetic field direction is changing this rapidly? I do not see anything in the datasheet that addresses this. Thanks.
Tomas,
Thanks for you response. I have several follow-up questions on this topic.
Thanks!
George
Hi George,
The main limitation is the maximum ODR which is 800Hz in magnetometer mode only. Considering your device rotates as fast as 7200 degrees/s, 1 sample corresponds to 9 degrees (7200/800), so the output would be in steps of 9 degree rotation. Noise needs to be taken into account at this ODR, as it increases with ODR. At 800Hz it reaches a typical 1.5uT rms which translates into a 3° rms uncertainty. So the FXOS8700CQ could be a good solution if accuracy requirement is not too stringent.
Regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.