Hi,
I have activated FlexBus in the CPU component. However, in the generated Code, all relevant pins are initialized to their correct alternative function (5 in my case), except for the CLKOUT pin (PORTC_PCR3), which has no initialization in Cpu.c
Is there a trick to activate that output?
PE Version: 10.3.0
Device: MK60FN1M0VLQ12
Thanks,
Martin
Solved! Go to Solution.
Hi Martin,
The CLKOUT pin control settings is availble in the CPU component in the Internal peripherals / System Integration Module / CLKOUT pin control. These properties are visible in the Advance or Expert view of Component Inspector window only, see the screenshot below:
Best Regards,
Marek Neuzil
Hi Martin,
The CLKOUT pin control settings is availble in the CPU component in the Internal peripherals / System Integration Module / CLKOUT pin control. These properties are visible in the Advance or Expert view of Component Inspector window only, see the screenshot below:
Best Regards,
Marek Neuzil