I am facing issue with IMX6 solo with 512 MB RAM, when I run GPU sample application with 512 MB ram it crashes after ~5-10secs. But the same crash doesn't happen for 1GB RAM. I suspect the memory range used for GPU is hard coded in the driver may cause the crash issue. To debug this i need source code for GPU driver(IMX6) Windows Embedded Compact 2013.
Can I get the source code for GPU driver (IMX6) Windows Embedded compact 2013?
AdeneoEmbedded , do you have information or can you help with this question?
Can you help me on this issue?