Andrew Ip

DDR RAM problem after lowering fsys of MCF5275

Discussion created by Andrew Ip on Sep 24, 2007
Latest reply on Oct 11, 2007 by Georg Brechlin
Hello,

we've tried to lower the fsys from 150MHz to 75MHz and the system will hang when it tried to copied data from the flash to the RAM and execute it. we're using u-boot and it works just fine when fsys is set within 100MHz and 150MHz. however, it hanged when we set the fsys to 75MHz or lower.

we only modified the the MFD & RFD in SYNCR while switching the fsys. so, we wonder if there's something else we need to modify?

- Inky Lung

Outcomes