AnsweredAssumed Answered

Problem with installing QorIQ-SDK-V1.4-SOURCE-20130625-yocto

Question asked by Victor Gomez on Nov 14, 2014
Latest reply on Nov 19, 2014 by Victor Gomez

Hi folks,I am running into a weird error when installing the QorIQ-SDK-V1.4-SOURCE-20130625-yocto.iso package.

 

I am installing it on my Fedora 20. And I did this:

 

1) Mounted the ISO

2) Executed the installation: /mnt/qoriq_yocto_1.4_source/install

3) CDed into the installation directory: <install_path>/qoriq-linux/fsc-sdk-1.4/QorIQ-SDK-V1.4-20130625-yocto

 

Up to here, everything worked like a charm, getting this message:

 

 

Done. You're ready to go with Yocto build now

250.207u 56.173s 34:07.18 14.9% 0+0k 3378300+5841776io 1363pf+0w

 

Now, I do the following:

source ./fsl-setup-poky -m p4080ds -j 12 -t 12 -l

 

And I get this error:

{local@host:55} source ./fsl-setup-poky -m p4080ds -j 12 -t 12 -l

Badly placed ()'s.

 

I get a "Badly placed ()'s error. I checked the fsl-setup-poky file, and I didn't see any misplaced () or any bug that was easy to see.

 

Do you have any ideas?

 

ANy help is much appreciated!
Thank you!
Best,
Victor.

Outcomes