Xfbdev

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,917 Views
alexandrglukhov
Contributor III

Hello, I have i.MX28 and I'm using Buildroot. Everything was ok, until I decide to clean file system with

make clean

and then make it again with

make.

Now, when I write:

Xfbdev -mouse tslib,2,device=/dev/input/event0 &

I get

Xfbdev: command not found

I think, I set the same configurations, but it seems, it different. Can you help me with it? Which package, library or element needs for Xfbdev working? Maybe need special version of gcc or other?

Labels (2)
Tags (2)
0 Kudos
1 Solution
1,392 Views
alexandrglukhov
Contributor III

There are two X.Org servers in buildroot: Modular and Tiny/Kdrive. If I first choose modular and then do make, I have no Xfbdev. And if then I change to another server, I still have no Xfbdev. But if I do make clean and choose Tiny/Kdrive - then I get my Xfbdev. So, it's ok now, thank you.

View solution in original post

0 Kudos
2 Replies
1,392 Views
b36401
NXP Employee
NXP Employee

I have no idea what went wrong.
Please try to put attached file into /usr/bin/ directory of root filesystem.

1,393 Views
alexandrglukhov
Contributor III

There are two X.Org servers in buildroot: Modular and Tiny/Kdrive. If I first choose modular and then do make, I have no Xfbdev. And if then I change to another server, I still have no Xfbdev. But if I do make clean and choose Tiny/Kdrive - then I get my Xfbdev. So, it's ok now, thank you.

0 Kudos