Multi-displays

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi-displays

Jump to solution
546 Views
thouswave
Contributor III

We are discussing a project which may need two 1080P displays,HDMI and LVDS.About these two interface,we have experience in using it on IMX6Q in previous project.Now we want to use it at the same time.

So I want to known if the IMX6Q chip can support two 1080P displays at the same time? If support,it can operate at which temperature without cooling device?

Labels (1)
0 Kudos
1 Solution
426 Views
igorpadykov
NXP Employee
NXP Employee

Hi 千 浪 .

yes, it is supported without problems.

Regarding temperature without cooling one can look at

AN4579 i.MX 6 Series Thermal Management Guidelines"

http://www.freescale.com/files/32bit/doc/app_note/AN4579.pdf

Best regards

igor

View solution in original post

0 Kudos
1 Reply
427 Views
igorpadykov
NXP Employee
NXP Employee

Hi 千 浪 .

yes, it is supported without problems.

Regarding temperature without cooling one can look at

AN4579 i.MX 6 Series Thermal Management Guidelines"

http://www.freescale.com/files/32bit/doc/app_note/AN4579.pdf

Best regards

igor

0 Kudos