Can I Flash a MC56F82313 using a USB Tap (Once) and the 56800E Flash Program?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I Flash a MC56F82313 using a USB Tap (Once) and the 56800E Flash Program?

1,837 Views
jeffreylefebre
Contributor I

I can't find a Device Config File for this device and I'm getting the error:  CCCSClient::ConfigChain: CC not present.

 

To call me a newbie to this is an understatement.

Labels (1)
2 Replies

1,426 Views
rogercox
Contributor I

Being unable to run 568000E Flash Programmer in Win10, I found an old Win7 machine that had been working from development 6 years ago.

But now, I get the "CCCSClient::ConfigChain: CC not present" error and don't know what it means.  I've tried downloading and installing afresh, but get the same error.  The FFLASH console is able to find the USB TAP, so that's not the issue

0 Kudos

1,426 Views
johnlwinters
NXP Employee
NXP Employee

There are three ways you can flash this device using tools available on freescale.com.

1) Use CW 10.6 to generate a project for the device and flash it with the debugger.

2) Generate an s-record file and flash it with the flash program invokable from the IDE of CW 10.6.

3) Use the DSC Flasher, a stand-alone programmer and select the device in "Target Device" to be MC56F82313.

This device is supported for all three methods.

0 Kudos