AnsweredAssumed Answered

MC56F826723/LP wait mode

Question asked by Audrey Eng Employee on Nov 6, 2014
Latest reply on Nov 10, 2014 by Ankur Kala

!In the LP Wait Mode, it says there that all peripheral modules are enabled, except NanoEdge and cyclic ADC’s. Is it also possible to configure the UART pin to change mode to be used as a GPIO during this mode of operation? If this is not possible, will the UART still operate in the same way that it does in normal run mode? Otherwise, what are some possible scenarios that could happen with the reduced clock frequency for the UART peripheral?

Outcomes