Hello,
Via JTAG I have loaded the CAN bootloader in the DSP56F8357, and now I need to load my application via CANBUS.
1- What steps is it necessary to realize the load?
Via JTAG I have loaded the CAN bootloader in the DSP56F8367 and now I need to load my application:
1 - what steps I have to do to load my application via CANBUS?
2 - How can I modify the BOOT START DELAY via CANBUS?
3 - which CAN -identifiers should be used?
I use IXXAT USB-to-CAN compact.
Thanks.
Modification of BOOT START DELAY is only at compile time given the design of the boot code.
Do you have the source? If so you can customize it.