Hi All,
CodeWarrior has this function: use the CodeWarrior Debugger to examine and modify data
http://www.freescale.com/files/training_pdf/24633_CW_DEBUGGER_DATA_WBT.pdf?lang_cd=ja
Does KDS have this function, too?
Because I can't add variables to variables windows in KDS.
Thanks.
Abby
Hi Abby,
KDS is using Eclipse Kepler, so this applies:
Variable Debugging with Eclipse Kepler | MCU on Eclipse
I hope this helps,
Erich
Hi Erich,
Thanks for your reply.
I need to modify variables but not view data only. (when CPU is running)
In KDS, I can add global variables to the expressions but can't modify the value when CPU is running.
The global variables only can be changed value when CPU is halt in KDS.
Abby
Hi Abby,
modifying variables while the target is running is a CodeWarrior specific extension, and not supported in stock Eclipse Kepler/CDT as used in Kinetis Design Studio.
See http://mcuoneclipse.com/2014/09/28/comparing-codewarrior-with-kinetis-design-studio/
Erich
Do you think that KDS will ever support these features? We switched to Freescale because of the advanced debugging including the ability use trace.
Until CDT will add that functionality, I'm affraid that KDS won't support this.