AnsweredAssumed Answered

iMX6 and LVDS

Question asked by Stefano Galeazzi on Nov 5, 2014
Latest reply on May 19, 2016 by berlin vince

Hi,

I have a RiotBoard, the external connection have a LVDS on miniHDMI connector 19pin.

The pin-out documented have 3 data LVDS signal (balanced line with N and P) configured TxData0, TxData1, TxData2.

 

I want to connect this Board with an LCD that have data input configurable to SELB to select 6bit or 8bit.

 

If I put the SELB on 6bit, I must use on LCD the RxData0, RxData1, RxData2 or the RxData1, RxData2, RxData3?

 

Thanks

 

Stefano

Outcomes