AnsweredAssumed Answered

What is this mean in u-boot, at sabrelite board?

Question asked by dayoung rho on Nov 4, 2014
Latest reply on Jun 25, 2015 by igorpadykov

Hello everyone.

 

Let me state my situation first.. I am a student who don't know well about sabrelite board.

So, I made a lot of horrible mistakes and I had to fix it. Finally I recovered my sabrelite and I got below lines:

What should I do next? I am very sorry about that my question is so ambiguous.

Any tiny advice will save my life!

 

----------------------------------------------------------------------------------------------------------------------------------

U-Boot 2014.04-00123-g63ae4a5 (May 14 2014 - 17:09:55)     

 

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz                                        
Reset cause: POR               
Board: SABRE Lite                
I2C:   ready           
DRAM:  1 GiB           
MMC:   FSL_SDHC: 0, FSL_SDHC: 1                              
MMC: no card present                   
MMC init failed              
Using default environment                        

No panel detected: default to HDMI                                 
Display: HDMI (1024x768)                       
In:    serial            
Out:   serial            
Err:   serial            
Net:   using phy at 6                    
FEC [PRIME]          
Warning: failed to set MAC address                                 
, usb_ether          
Hit any key to stop autoboot:  0                               
MMC: no card present                   
mmc0(part 0) is cur                
MMC: no card present                   
Booting from net ...                   
FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !                                                                  
*** ERROR: `ethaddr' not set                           
ERROR: Need valid 'usbnet_devaddr' to be set                                           
at drivers/usb/gadget/ether.c:2362/usb_eth_init()                                                
FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !                                                                  
FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !                                                                  
*** ERROR: `ethaddr' not set                           
ERROR: Need valid 'usbnet_devaddr' to be set                                           
at drivers/usb/gadget/ether.c:2362/usb_eth_init()                                                
FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !                                                                  
Wrong Image Format for bootm command                                   
ERROR: can't get kernel image!                             
----------------------------------------------------------------------------------------------------------------------------------

Outcomes