Hi Takashi
yes this will be supported
correct will be 640*480 pix*30fps*2camera=18.432Mpix/sec.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your support.
I have 3 additional questions.
1, Description of IMX6SDL RM of Table 38-29.
IPU's capture flows 『Capturing interlaced input and
storing it in the memory (via VDIC) while performing video de-interlacing in
the VDIC.』 in 『Interlaced input coming from one of the CSIs is sent to the memory without processing via channel #13.
Below in my understanding is correct?
Table 38-9 listed IDMAC DMA channels list, IDMAC_CH_13 at the VDIC Source and Destination are Fmem.
However, correct in understanding that the real CH_13 at the CSI Source, Destination Fmem, en route via the VDIC, so Source listed the VDIC?
And Using a CH_13, CSI → VDIC transfer, without the IDMAC of another channel?.
2, In the VDIC, without any De-interlacing On the Fly,
That is correct understanding?
When capturing simultaneously CSI1, both CSI0 and CSI1 using IDMAC CH_13 into the via the VDIC Fmem.
And VDIC is de-interlacing at once only of 1 ch, even if can be relay to the above CSI → Fmem and will be 2ch at the same time?
3, When capturing BT.656 from CSI1, CSI0 2-channel sametime, route and IDMAC channel in the below mentioned correct?
Hi Takashi
for new subject please create new Community thread.
Best regards
igor