Hi all,
I'm using the i.MX6Q Sabre Lite Board to test some algorithms and would like to know if there is any tool that can assist me in collecting data, such as processing time and the resources used (CPU, GPU).
Thanks in advance,
Douglas
Hello Douglas,
I can only recommend that you use the TOP linux command so you can get the information that you are trying to accomplish, here is a link, that can help:
Unbelievable ! 30 Linux TOP Command Examples With Screenshots
For the GPU you can use the VProfiler, that it is a tool from the Vivante SDK, you can download it from the following link:
I.MX_6_VIVANTE_VDK_150_TOOLS , just a little advise, this is tool it is made for the Freescale BSP since you are using the SABRE Lite board from Nitrogen. You need to check if the GPU it is enable in your kernel.
saludos