Hello community,
regarding to the AN4784 (http://cache.freescale.com/files/32bit/doc/app_note/AN4784.pdf) you have a "Maximum transition eye voltage: 0.376 volts". The boundary values to pass this testcase are ''257.000 mV < x < 600.000 mV".
I have a couple of questions, pls feel free to answer them:
Regards
Hi ro
I would suggest to ask local FAE provide PCIe report for you from
internal link
iMX6DL PCIe compliance test report
Best regards
igor
Hi igorpadykov,
basicay after a lot of reading I can answer all questions by my self.
But nevertheless, the VDD_SoC Voltage depends on the ARM PLL clock. If the PCIe Phy is supplied from the VDD_SoC voltage (imx6S LDO) I have to change the values on the IOMUXC_GPR8 register.
What is the expected voltage drop between the settings in IOMUXC_GPR8 (PCS_TX_SWING_FULL) register and the expected voltage value at the imx6 ball?
regards
Hi ro
VDD_SoC Voltage does not depend on the ARM PLL clock, it may
depend on VPU frequency. Please check Table 9. Operating Ranges
Reagrding "expected voltage drop between the settings" I am not
sure if that was measured/characterized.
~igor