iMX6DL : How to set the PCIe PHY Reference Clock source ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6DL : How to set the PCIe PHY Reference Clock source ?

Jump to solution
1,017 Views
koichisakagami
Contributor II

Dear community,

I consider using i.MX6DL PCIe PHY
Please see Table 50-1 (p.4455) in IMX6SDLRM (Rev.1).

I hope use the  CLK1(In)  to "Reference Clock" as a clock source
with the following setting.

Is my understanding correct ?

CCM_ANALOG_PLL_ENETn (pp.909-911)
  ENABLE_100M:0x1
  BYPASS_CLK_SRC:0x1
  BYPASS:0x1

PMU_MISC1n (pp.4528-4530)
  LVDSCLK1_IBEN:0x1
  LVDSCLK1_OBEN:0x0

PCIE_PHY_MPLL_ASIC_IN (pp.4470-4471)
  MPLL_MULTIPLIER:0x19

PCIE_PHY_ATEOBRD_STATUS (pp.4474-4475)
  REF_CLKDIV2_IN:0x0

If some adittional setting is required, could you let me know it ?

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
1 Solution
634 Views
igorpadykov
NXP Employee
NXP Employee

Hi koichi

I think that understanding is correct and

these settings are sufficient for external clock.

Also one can refer to example below

i.MX6Q: Using an external reference for PCIe

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
635 Views
igorpadykov
NXP Employee
NXP Employee

Hi koichi

I think that understanding is correct and

these settings are sufficient for external clock.

Also one can refer to example below

i.MX6Q: Using an external reference for PCIe

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
634 Views
koichisakagami
Contributor II

Dear igor san,

With the following setting,
does the CLK2(out) output the  "Reference Clock"  ?

PMU_MISC1n (pp.4528-4530)
  LVDS2_CLK_SEL : 0b01010 (PCIE_REF)

"Reference Clock" is defined at

Table 50-1 (p.4455) in IMX6SDLRM (Rev.1).

Best Regards,

Koichi Sakagami

0 Kudos