MFG tool has been released for Windows CE.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG tool has been released for Windows CE.

914 Views
jamesko
Contributor I

Hi!

I need the MFG tool for Windows CE.

I'm going to test you to download WEC7 OS image on a custom board (IMX6Q).

Those who have the information, please help me to.

Thanks. 

James

Labels (2)
0 Kudos
2 Replies

541 Views
SergioSolis
NXP Employee
NXP Employee

Hello James,

Unfortunately MFGTool is not programmed to flash Windows to our Boards.

541 Views
jamesko
Contributor I

Hi!

Thank you reply.

Below WEC7 OS image was being downloaded to iMX53 to Mfgtools-Rel-1.6.2.048,

1. that may be used to fix this?

File = ucl.xml


<UCL>
  <CFG>
    <STATE name="BootStrap" dev="MX53" />
    <DEV name="MX53" vid="15A2" pid="004E"/>   
    <STATE name="Updater"   dev="Updater" /> 
    <DEV name="Updater" vid="066F" pid="37FF" />
  </CFG>
  <LIST name="NAND" desc="Choose NAND as media">
   <CMD type="find" body="BootStrap" timeout="300"/>
        <CMD type="boot" body="BootStrap" file ="eboot_uut.nb0" >Running plugin to init DDR Memory.</CMD>        
        <CMD type="load" file="uce.nb0" address="0x70200000" loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Doing preLoad."</CMD>      
        <CMD type="jump" > Jumping to OS image. </CMD>
        <CMD type="find" body="Updater" timeout="300"/>
        <CMD type="push" body="MediaType:NAND">Send media type.</CMD>
        <CMD type="push" body="QueryStoreName:NAND FLASH Storage,Timeout:10">Query store name.</CMD>                         
        <CMD type="push" body="wfw">Notity device to prepare receiving a firmware.</CMD>
        <CMD type="push" body="fwtype:EB_NB">Specify firmware type.</CMD>
        <CMD type="push" body="send" file="files/eboot.nb0">Sending a firmware file.</CMD>
        <CMD type="push" body="save">write the firmware to NAND flash.</CMD>   
        <CMD type="push" body="wfw">Notity device to prepare receiving a firmware.</CMD>
        <CMD type="push" body="fwtype:NK_NB">Specify firmware type.</CMD>
        <CMD type="push" body="send" file="files/nk.nb0">Sending a firmware file.</CMD>
        <CMD type="push" body="save">write the firmware to NAND flash.</CMD>
        <CMD type="push" body="QueryFolderStatus:NANDFlash,Timeout:10">Query store folder status.</CMD>
        <CMD type="push" body="wfl">Notity device to prepare receiving a file.</CMD>
        <CMD type="push" body="filename:NANDFlash\\sandy.mp3">Sending file name.</CMD>
        <CMD type="push" body="send" file="files/sandy.mp3">Sending a file.</CMD>   
        <CMD type="push" body="save">Finish sending data.</CMD>                                                
        <CMD type="push" body="Done">Whole update work is finished.</CMD>
        <!--<CMD type="push" body="ResetBoard">Reset the board to start next round test.</CMD>-->
  </LIST>
    <LIST name="SD/MMC" desc="Choose SD/MMC as media">
<CMD type="find" body="BootStrap" timeout="60"/>
        <CMD type="boot" body="BootStrap" file ="eboot_uut.nb0" >Running plugin to init DDR Memory.</CMD>        
        <CMD type="load" file="uce.nb0" address="0x70200000" loadSection="OTH" setSection="OTH" HasFlashHeader="FALSE" >Doing preLoad."</CMD>       
        <CMD type="jump" > Jumping to OS image. </CMD>
        <CMD type="find" body="Updater" timeout="180"/>
        <!--<CMD type="push" body="FuseRead:0x00000860">read fuse value.</CMD>
        <CMD type="push" body="FuseSense:0x00000860:0x00000003">read fuse value.</CMD>
        <CMD type="push" body="FuseProgram:0x00000860:0x00000010">read fuse value.</CMD>-->               
        <CMD type="push" body="MediaType:SDMMC">Send media type.</CMD>
        <!--<CMD type="push" body="QueryStoreStatus:DSK2:,Timeout:10">Query store status.</CMD>-->
        <CMD type="push" body="QueryStoreName:SD Memory Card,Timeout:10">Query store name.</CMD>
      <CMD type="push" body="Partitions:Firmware:100MB,File">Starting partitions.</CMD>     
        <CMD type="push" body="wrd:0x400">Write raw data to device with a specified starting address.</CMD>
        <CMD type="push" body="send" file="files/eboot.nb0">Sending a file.</CMD>
        <CMD type="push" body="save">Finish sending data.</CMD>     
        <CMD type="push" body="wrd:0x80400">Write raw data to device with a specified starting address.</CMD>
        <CMD type="push" body="send" file="files/nk.nb0">Sending a file.</CMD>
        <CMD type="push" body="save">Finish sending data.</CMD> 
        <CMD type="push" body="QueryFolderStatus:SDMemory,Timeout:10">Query store folder status.</CMD>
        <CMD type="push" body="wfl">Notity device to prepare receiving a file.</CMD>
        <CMD type="push" body="filename:SDMemory\\sandy.mp3">Sending file name.</CMD>
        <CMD type="push" body="send" file="files/sandy.mp3">Sending a file.</CMD>
        <CMD type="push" body="filename:SDMemory\\DWS.exe">Sending file name.</CMD>
        <CMD type="push" body="send" file="files/DWS.exe">Sending a file.</CMD>         
        <CMD type="push" body="save">Finish sending data.</CMD>      
        <CMD type="push" body="Done">Whole update work is finished.</CMD>
    </LIST>   
</UCL>

0 Kudos