Hello,
I am using iMX6S procesor in our board. We could program Eboot+NK.bin into the eMMC. But couldn't boot the board from eMMC. I am getting below error when I compared the logs with working board while programming.
Could you suggest the solution ?
Old situation:
Warning: The partition table looks like it was made
for C/H/S=*/1/0 (instead of 461824/1/16).
For this listing I'll assume that geometry.
Regards,
Azlum
hello Mohammed,
Are you trying to install a windows release?, did you download it from a third party company?
Hi Serch,
We are trying to program WEC7 [also tied with Linux BSP]. But the result is any BSP [Linux/Android/Linux] not able to boot from eMMC.
Note that, I could boot the same board from SD card. After booting I could access the user area of eMMC, which means I could copy and paste contents to and from eMMC.
Regards,
Azlum