PHY-IC to use i.MX6Q IEEE1588 function.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PHY-IC to use i.MX6Q IEEE1588 function.

Jump to solution
813 Views
satoshishimoda
Senior Contributor I

Hi all,

We consider the use of IEEE1588 for time synchronization in the Ethernet function.

We know i.MX6Q datasheet(MAC) is written as supporting IEEE1588.
To use IEEE1588, should external PHY-IC support IEEE1588 function also not only i.MX6Q?

Also if PHY-IC should support IEEE1588, do you know recommended PHY-IC product other than "AR8031"?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (2)
0 Kudos
1 Solution
580 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes, external PHY-IC should also support IEEE1588 function.

You can use any RGMII PHY-IC, since this is standard interface.

Freescale cannot recommend one supplier over another and does

not suggest that this is the only phy supplier.

Best regards

igor
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
581 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes, external PHY-IC should also support IEEE1588 function.

You can use any RGMII PHY-IC, since this is standard interface.

Freescale cannot recommend one supplier over another and does

not suggest that this is the only phy supplier.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos