Hi to all,
I've a small project with KE02 and SD Card on SPI peripheral, without SO.
I use Fat_FileSystem bean that uses SD card beans and others.
When I build the project I've some errors, in SD1.c file.
you can see
Description Resource Path Location Type
'SM1_DeviceData' undeclared (first use in this function) SD1.c /PDD/Generated_Code line 461 C/C++ Problem
Regards,
Paolo Colombo
Solved! Go to Solution.
Hi Paolo,
thinking more about it, I think you missed to select 'auto initialization' in the SM1 component:
This will create the SM1_DeviceData in the SM1.h header file.
Erich
Hi Paolo,
Have you configured two speed modes for the SPI?
See http://mcuoneclipse.com/2012/11/18/arduino-data-logger-shield-with-the-frdm-kl25z-board/
I hope this helps,
Erich
Hi Paolo,
thinking more about it, I think you missed to select 'auto initialization' in the SM1 component:
This will create the SM1_DeviceData in the SM1.h header file.
Erich