AnsweredAssumed Answered

USBDM & CW10.6: Launch Configuration Migration to RSE Required -> failed!

Question asked by GUITTET JOEL on Oct 17, 2014
Latest reply on May 11, 2016 by Ankur Patel

Hello all!

 

I'm a little bit confused. I have just made a fresh installation of CodeWarrior 10.6 with an USBDM upgraded to 4.10.6.200 and drivers 1.3.0 (thus all the last releases) and I have created a new project in a new workspace. I'm getting this message "Launch Configuration Migration to RSE Required" when clicking the "Finish" button of the project creation wizard.

 

migration required.PNG

 

Then click "OK" I get the following error:

 

migration failed.PNG

 

I can create and build my application in CodeWarrior but it is not possible to launch debug: target is not defined as shown below:

 

no target.PNG

 

Any ideas ?

 

My configuration is the following:

- Windows 7 x64;

- CodeWarrior installed in "C:\Program Files (x86)\Freescale\CW MCU v10.6" directory;

- USBDM 4.10.6.200 with drivers 1.3.0;

- Target S08DZ60.

 

Previously I was working with CW10.6 and USBDM 4.10.6.140B and drivers 1.2.0 on the same computer and I never get this kind of issue.

 

Regards,

Joel

Outcomes