Wifi access point on k60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wifi access point on k60

482 Views
jean-francoisle
Contributor III

Hi everyone,

Our application is develop on K60DN512 (with MQX 3.7). There is a cellular modem that supply the connectivity to internet. On this part, everything works fine. We want to develop an expansion board with wifi (radio or modem, without or whitout embed stack). This expansion board must offer an access point (hot spot) having the internet with our MCU/cellular modem. We can add an MCU if we need more processing. There is 4 towers that offer wifi (gainstan, redpine, atheros). There is a patch for MQX 3.7 for those radios. My question is the following: In the stack, is it possible to cofigure the device as an access point? Is there an app notes to do something like this?

Any suggestions?

Regards,

JF

Labels (1)
0 Kudos
1 Reply

328 Views
Masmiseim
Senior Contributor I

hey,

Here is a discussion about "Soft-AP" and Wi-fi Direct with the Atheros AR4100:

TWR-WIFI-AR4100 patch supprt wifi direct?

Regards

Markus

0 Kudos