Hi Arctic
please refer to attached i.MX51 WinCE60 Manual p.128
sect.11.2 "Supported Functionality" :
"The eSDHC driver enables the hardware to provide the following software and hardware support:
..
SD, SD High Capacity (up to spec v2.1), MMC (up to spec v4.3), and SDIO cards (up to spec v2.0).
High capacity MMC cards are not supported because SDBUS2 in CE 6.0 R2 does not support these
cards."
klm8g2fe3b is rev.4.41 and not supported, sorry.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------