Hi team,
My customer is considering the implementation of workaround#2 for errata ERR006282 of i.MX6.
And they have a question on the workaround#2 of ERR006282.
Could you show me how to turn off the watchdog timer specifically?
Thanks,
Miyamoto
Hi AVNET JAPAN FAE (team share account)
once enabled WDog can not be disabled.
From sect.70.7.1 Watchdog Control Register (WDOGx_WCR) IMX6DQRM
WDT,WDE is a write one once only bit.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
The following description is written in the errata document(IMX6DQCE Rev.4).
Note: If the WDOG_ENABLE fuse is set, users who utilize the Freescale
Manufacturing Tool or a customized version of the tool must ensure the
kernel that is downloaded via the tool contains the instruction to turn off the
watchdog timer. Otherwise, the watchdog will continue to count down and
reset the part.
Does the "instruction to turn off the WDT" mean reloading the timer, or things like that?
BestRegards,
Miyamoto
Hi Miyamoto
seems "instruction to turn off the WDT"
is misprint, since it is not possible to turn off
WDT once enabled, according to RM
sect.70.7.1 Watchdog Control Register (WDOGx_WCR) IMX6DQRM
WDT,WDE is a write one once only bit.
Best regards
igor
Hi Igor,
I think it must include the instructions to make WDT not expired, rather than 'turn off the WDT'.
Correct?
BR,
Miyamoto
Hi Miyamoto
yes I think this is correct.
Best regards
igor