P2020 LALE Output Delay

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 LALE Output Delay

Jump to solution
552 Views
stevenrendano
Contributor I

P2020EC Rev 2, Table 59, Enhanced Local Bus Timing Specifications - PLL Enabled Mode, does not provide output delay for LALE.  Associated Figure 37, Local Bus AC Timing Diagram (PLL Enabled), shows LALE output delay less than general output delay tLBKHOV.  Is this relationship guaranteed, i.e. is LALE output delay always less than or equal to tBKHOV?

Labels (1)
Tags (4)
0 Kudos
1 Solution
399 Views
alexander_yakov
NXP Employee
NXP Employee

LALE timing is specified relatively to LAD - timing parameter tLBONOT

LALE is used to drive external address latch, so the only required parameter for latch is hold time for LAD signals relatively to LALE negation.

We do not specify other timings for LALE.

View solution in original post

0 Kudos
1 Reply
400 Views
alexander_yakov
NXP Employee
NXP Employee

LALE timing is specified relatively to LAD - timing parameter tLBONOT

LALE is used to drive external address latch, so the only required parameter for latch is hold time for LAD signals relatively to LALE negation.

We do not specify other timings for LALE.

0 Kudos