AnsweredAssumed Answered

Debugging with hexfile

Question asked by bob_walker on Oct 7, 2014
Latest reply on Oct 10, 2014 by Pascal Irrle

I have a boot loader that updates the user application via SCI.

The application runs fine when compiled stand alone. However when running with the boot loader, its behavior is erratic.

The boot loader clears all memory, my application uses no static variables, and I'm not using any CW libraries.

After loading the new image into flash, I can see that the code and its interrupts are mapped where they should be.

 

What I'd like to do is to connect to the target via a debug configuration (CONNECT?) that will not disturb the image and

will use the application's symbols for debugging. Is this possible? If so, how?

Outcomes