Compiling the libs for TWRK60D512 and many undefined symbols in BSP_CM.c.
This is clean fresh install of MQX and IAR. TWRK60D100M builds fine.
Has anyone else experienced this?
Error[Pe020]: identifier "MCG_ATC" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 205
Error[Pe020]: identifier "MCG_ATC" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 208
Error[Pe020]: identifier "MCG_ATC" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 210
Error[Pe020]: identifier "MCG_ATC_ATME_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 210
Error[Pe020]: identifier "MCG_ATC" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 212
Error[Pe020]: identifier "MCG_ATC_ATMF_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 212
Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 349
Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 389
Error[Pe020]: identifier "MCG_S_LOCK_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 403
Error[Pe020]: identifier "MCG_S_LOCK_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 422
Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 450
Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 514
Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 551
Error[Pe020]: identifier "MCG_S_LOCK_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 820
Error[Pe020]: identifier "MC_PMCTRL" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 836
Error[Pe020]: identifier "OSC_CR" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 913
Error[Pe020]: identifier "MCG_S_LOCK_MASK" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 952
Error[Pe020]: identifier "LLWU_CS" is undefined D:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk60n512\bsp_cm.c 1021
Hi John,
Unfortunately I cannot to reproduce your issue. I am using MQX4.1.1 and IAR 7.1.
According with the release notes, Freescale MQX RTOS was compiled and tested with IAR Embedded Workbench® for ARM® Version 7.10.3.
Did you try using IAR 7.10??
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------