PCB design of daughter cards for MC9S08QE128 and MCF51QE128 microcontrollers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCB design of daughter cards for MC9S08QE128 and MCF51QE128 microcontrollers

423 Views
juancarlossuare
Contributor III

Hello.

 

I need a schematic and a PCB design of daughter cards for MC9S08QE128

and MCF51QE128 microcontrollers. These daughter cards are part from

DEMOQE128, and are two interchangeable plug-in daughter cards to

quickly evaluate the 8-bit S08 and 32-bit ColdFire V1 QE128 MCUs.

 

I could not get these Daughter Cards. I need these parts to work with my

DEMOQE128.

 

¿Can you provide these design files?

 

Thanks .

Labels (1)
0 Kudos
1 Reply

305 Views
arpitaagarwal-b
NXP Employee
NXP Employee

Hello Juan,

Download DEMOQE128SCH from this link: MCF51QE128 Demonstration Board|Freescale

The zip folder has some daughter card related files.

Please see if these are the files you are looking for?

If this post helps you, kindly mark it as correct/helpful answer.

-Arpita

0 Kudos