Bluetooth Low Energy v4.1 Role Switching

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bluetooth Low Energy v4.1 Role Switching

1,029 Views
kelvinleung
NXP Employee
NXP Employee

One of the key enhancements for BLE in v4.1 is the added support for a slave device to be able to connect to TWO master devices, i.e., the slave device can simultaneously belong to two star networks. This was not allowed in v4.0 specification.

A slave device can also act as a bridge between two star networks. However, this is not explicitly covered in v4.1 of the spec. The topic of a slave devices to act as a bridge between two star networks and the master-slave role-switching are expected to be resolved in future versions of the specification.

Tags (1)
0 Kudos
0 Replies