New sensor driver: board_mx6q_sabresd.c is missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New sensor driver: board_mx6q_sabresd.c is missing

Jump to solution
1,180 Views
andreatessadri
Contributor I

I am writing a new driver to support a new sensor Aptina MT9J003 and I am following the BSP Porting Guide.

When I came to the point to add a new platform_data structure into the I2C bus, I cannot find in my build environment the file board_mx6q_sabresd.c as mentioned into the BSP Porting Guide.

I have properly created the build environment with export MACHINE="imx6qsabresd" (that is also the default configuration) but as well I cannot find in <build-dir>/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/driver/arch/arm  (and subdirs ...) any file board_imx6q_*.

Thank you in advance

   Andrea

Labels (4)
0 Kudos
1 Solution
691 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andrea

please look at yocto docs, i.MX_6_BSP_Porting_Guide.pdf

L3.10.17_1.0.0_LINUX_DOCS   Linux 3.10.17 BSP & MM Bundle

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
5 Replies
691 Views
sanjayanand
Contributor II

Hey Andrea,

We were also planning to port from MT9P006 to MT9J003

If it is okay could you please share the driver code??

Thanks in advance. :smileyhappy:

Regards,

Sanjay Anand

0 Kudos
692 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andrea

please look at yocto docs, i.MX_6_BSP_Porting_Guide.pdf

L3.10.17_1.0.0_LINUX_DOCS   Linux 3.10.17 BSP & MM Bundle

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
691 Views
andreatessadri
Contributor I

Thanks Igor for this documents.

What I don't know is how to understand which is my board name. Actually is IMX6Q-SabreSD but I cannot figure out where is the .c file calling the board_init function.

Could you help me ?

Thanks

  Andrea

0 Kudos
691 Views
fabio_estevam
NXP Employee
NXP Employee

If you are using kernel 3.10 then there are no board files anymore. These were replaced by device tree.

Take a look at arch/arm/boot/dtx/imx6qdl-sabresd.dtsi

691 Views
andreatessadri
Contributor I

Thanks both of you guys, I've got now that the doc bundle refers to the new kernel.

So the dts file replaces the board file.

0 Kudos