AnsweredAssumed Answered

dev-pkgs tools-sdk in nitrogen6x build

Question asked by Niklas Molin on Sep 29, 2014

Hi.

 

I'm trying to build for my sabrelite board in Yocto (using machine nitrogen6x).

I'm trying to include the gcc compile, tools etc., so I add following lines in my local.conf file

IMAGE_FEATURES += " \

   dev-pkgs \

    tools-sdk \

"

 

But I get an error when I compile with this features (using core-image-base image):

ERROR: QA Issue: package libxml-parser-perl contains bad RPATH ...../build/tmp/sysroots/nitrogen6x/usr/lib in file ...../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxml-parser-perl/2.41-r3/packages-split/libxml-parser-perl/usr/lib/perl/vendor_perl/5.14.3/auto/XML/Parser/Expat/Expat.so

ERROR: QA run found fatal errors. Please consider fixing them.

ERROR: Function failed: do_package_qa

ERROR: Logfile of failure stored in: ...../build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/libxml-parser-perl/2.41-r3/temp/log.do_package.11612

ERROR: Task 2598 (...../sources/poky/meta/recipes-devtools/perl/libxml-parser-perl_2.41.bb, do_package) failed with exit code '1'

 

Is there anything I'm missing here?


Best regards,

Niklas

Outcomes