DC coupling on the SGMII receiver.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DC coupling on the SGMII receiver.

634 Views
al123
Contributor I

On our P4080 design we have DC coupling on the SGMII receiver.
It is driven by a CML output stage power by 1.4Volts. The XVDD voltage on our
design is 1.5 Volts. Table 88 does not specify a DC Input voltage range. Do you
happen to have a value for this? Do you think this will be a issue since the
driver is at 1.4 Volts?

Labels (1)
0 Kudos
1 Reply

373 Views
r8070z
NXP Employee
NXP Employee

Table 88 does not specify a DC input voltage range because it says "Input must be externally AC coupled." I think you should change to AC coupling, otherwise you violate P4080 electrical specifications requirement.

0 Kudos