AnsweredAssumed Answered

ADC Module

Question asked by Pascal Schröer on Sep 26, 2014
Latest reply on Sep 26, 2014 by Pascal Schröer

Hi at all,

 

My device: MK10DX128VLH7

 

I have got two questions:

 

1. Is there only a 12bit instead of a 16bit ADC module used? So I can only get a 16bit resolution with the help of oversampling?!

 

2. Can I reach the full resolution if I use an external 2.5V reference? I made some experience with the freescale S12 series and there I have to use a 3V reference to get the full resolution?!

 

 

Thanks :)

 

Pascal

Outcomes