AnsweredAssumed Answered

i.MX6SDL VDD_ARM_CAP LDO output set point @ 996MHz.

Question asked by Satoshi Shimoda on Sep 25, 2014
Latest reply on Sep 28, 2014 by Yuri Muhin

Hi community,

 

Our partner have a question about i.MX6SDL operating range.

Please see Table 9 in IMX6SDLCEC Rev.3.

LDO Output Set Point (VDD_ARM_CAP) when LDO enabled mode is same as VDD_ARM_IN(min) at operation up to 792MHz and up to 396MHz.

However, LDO Output Set Point = 1.225V and VDD_ARM_IN(min)@ up to 996MHz = 1.250V.

These are not same value.

We guess LDO Output Set Point = 1.225V @ up to 996MHz when LDO enabled is misprint, and correct value is 1.250V.

Is this correct?

 

 

Best Regards,

Satoshi Shimoda

Outcomes