I creat a BSP clone, but at Libraries build project, it does not contain the project file.
I check the filesystem, I find there are something missing:
I assume {MQX_ROOT}=D:\Freescale\Freescale_MQX_4_1 , {BOARD_NAME}=CIRL_k60f150m , copy from {BOARD_SOURCE}=twrk60f120m, IDE is CW10.6
In the path {MQX_ROOT}\build\{BOARD_NAME}\cw10gcc\ , the wsd file does contain the ffs project declaration, but does not have such BOARD_NAME(directory) in {MQX_ROOT}\ffs\build\cw10gcc\ .
I try to do something with this issue, and find some solution:
Copy the directory by using the {BOARD_SOURCE} as template which you clone from, and rename it to {BOARD_NAME} , then search all sub-directories and find every file which contain the string {BOARD_SOURCE}.
Replace it ( {BOARD_SOURCE} ) to {BOARD_NAME}.
Then, when you use the CodeWarrior, using the work set import, it goes well!
I use the same method, to build my KDS project.
I referenced the guide books of MQX. Especially the MQX_User_Guide
Hi Wang,
On 24-Oct we have released patch for MQX 4.1.1 which adds KDS support to “BSP Cloning Wizard”.
It’s available to download in “Updates and Patches” section: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX&fpsp=1&tab=Design_Tools_Tab
=================================
this answer is for you, if it helps, please click on "Correct Answer" button, thanks!
Best Regards,
Zhang Jun
I experienced the same issue with MQX 4.1. The "ffs\examples" and "ffs\source" folders were copied, however the "ffs\build" directory was omitted. I manually created the "build\iar\<board name>" folder structure, copied the reference board files, and then renamed them. Note that I had selected to only generate the IAR projects (ARM DS-5 option was unchecked).
It was unclear to me from Zhang Jun's reply whether the MQX 4.1.1 patch fixes the ffs cloning issue.
FFS issue was fixed by MQX 4.1.1 Cloning Wizard Patch.
Thank you for your report.
I will report it (missing ffs support in BSP clonning wizzard) to our internal bug/task database.
We are currently working on BSP cloning Wizzard update and I suppose, that this new feature will be added in one of next releases.
Have a great day,
RadekS