AnsweredAssumed Answered

In USB USBRST bit is not getting set.

Question asked by shabana m on Sep 24, 2014
Latest reply on Sep 25, 2014 by Kan_Li

Hi,

The following are the things that I have done.

     1. Im using the Freescale USB stack v4.1.1.

     2. The example project that Im refering is msd_msf_generic -> K40.

     3. Im converting the K40 project to KL46.

     4. In not using the same workspace to create the project instead I have copied the files to some other workspace.

 

The problem is if I connect the USB memory stick the control comes to the ISR but the USBRST bit is not set.

The register looks like the attached picture.

can any one help me!!!!!!!

 

Regards,

Shabana

Attachments

Outcomes