When downloaded the Evaluation: CodeWarrior for MPC5xx v8.7 fails during installation, (windrvr6.inf file missing)
Tried the CW of MPC55xx evaluation - that installed fine.
(On windows 7 service pack1 32-bit system).
Is there any chance to install that evaluation?
Thank you Fiona,
I was aware of that note you are pointing, but there was written Win7 64bit - so I was thinking by mistake, that the Win7 32-bit will be ok.
The installation of virtual PC worked. I also tried to move that copy to Win7 and it seems working also.
Unfortunately CodeWarrior for MPC5xx V8.7 is not working on Win 7. It is a 32-bit application. Please view the note on its webpage:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MPC5XX
We recommend to use Windows 2000, Windows XP/Vista (32-bit).
These are the official OS supported.
At this time there is no plan for a new version supporting Win 7.
There are two workarounds:
1)- install it on win XP,
- copy installation under win 7,
- install new P&E driver if needed
2) if the above will not work the other solution will be the virtual PC.
Best Regards
Fiona
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------