Hi All,
I am using IMX51 and boot it from SD/MMC(klm8g2fe3b-b001) successfully,but someday i make a wrong eboot menu lead to uable to restart and no output in serial console,but I can burn burn right image file byAdvanced tookit successfully.why?
Wrong eboot menu configuration that i make,below.
-----------------------------------------------------------------------------
Freescale iMX SOC Menu Item
-----------------------------------------------------------------------------
[0] IP Address : 0.0.0.0
[1] Set IP Mask : 0.0.0.0
[2] Boot Delay : 3
[3] DHCP : Disabled
[4] Reset to Factory Default Configuration
[5] Select Boot Device : NK from SD/MMC
[6] Set MAC Address : FF-FF-FF-FF-FF-FF
[7] Format OS NAND Region
[8] Format All NAND Regions
[9] Bootloader Shell
[I] KITL Work Mode : Interrupt
[K] KITL Enable Mode : Disable
[P] KITL Passive Mode : Disable
[S] Save Settings
[D] Download Image Now
[L] Launch Existing Flash Resident Image Now
[E] Select Ether Device : FEC
[M] MMC and SD Utilities
Selection: M
-----------------------------------------------------------------------------
Freescale iMX SOC Menu Item
-----------------------------------------------------------------------------
[A] eMMC 4.3 Boot Partition : Disabled / Not Available
[B] eMMC 4.3 Boot Partition Size : 2048 Kbytes
[S] eSD 2.1 Boot Partition : Disabled / Not Available
[D] eSD 2.1 Boot Partition Size : 0 Kbytes (error chose)
[C] Create File System Partition on SD/MMC Boot Card (right chose)
[F] Format All SD/MMC Regions
[R] Return to Main Menu
Right chance is C,but I chose the wrong chance A or Bor Sor D,I can't remeber it.when i chosed it ,the board can't start normally,and a serial port can't print anything,but I can burn burn right image file by Advanced tookit successfully in download mode.why?
Thanks,
Arcatus
Solved! Go to Solution.
I think you could try to experiment with different eMMC
and find reason what is wrong. If you are using eMMC 4.41
(klm8g2fe3b-b001) which is not supported by i.MX51 (according
to documentation) you can not expect normal operation.
~igor
Hi Arctic
ATK ToolKit just perform raw writing to SD sectors, it runs without OS and do not use partitions
info. While MFG Tool is small linux image it expect to see SD card among its devices.
To answer your question it is necessary to know what exact manipulations you
did, so it may be recommended just to try reproduce this issue once more time.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi igorpadykov
Wrong choose lead to be unable to start and serial port can't print any information,how should i do with?
I think you could try to experiment with different eMMC
and find reason what is wrong. If you are using eMMC 4.41
(klm8g2fe3b-b001) which is not supported by i.MX51 (according
to documentation) you can not expect normal operation.
~igor
I will follow your suggestion,and have a try.
thanks,
Arctic